Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is it possible to obtain 90 degree temperature rated lugs for an 1200A I-Line panel?
Issue:
Temperature rated lugs for a 1200A I-Line panel.

Product Line:
I-line panelboards.

Environment:
Products sold in the United States.

Cause:
Product features.

Resolution:
All of the I-Line panel lugs are 75 degrees listed, we have no available 90 degrees lugs or options for listing at 90 degrees.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings