Issue:
Are motor circuit protectors, or Mag Gard Breakers UL 489 listed?
Product Line:
Circuit Breakers
Resolution:
Motor circuit protectors do not have a UL 489 listing per se, but are a UL recognized component for use in a motor control application in conjunction with a thermal overload component.
Are motor circuit protectors, or Mag Gard Breakers UL 489 listed?
Product Line:
Circuit Breakers
Resolution:
Motor circuit protectors do not have a UL 489 listing per se, but are a UL recognized component for use in a motor control application in conjunction with a thermal overload component.
Released for: Schneider Electric USA