Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the endurance on the motor operators for the H and J frame breakers?
Issue:
Endurance of the motor operator for H-frame

Product Line:
Molded Case Circuit Breaker

Resolution:
The motor operator endurance for the H and J frames is 5000 operations.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings