Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the part numbers for finger safe lug covers for Powerpact H and J frame breakers?

Article available in these languages: Korean

Issue:
Looking for IP20 terminal shields for H and J frame circuit breakers

Product line:
Molded case circuit breaker accessories

Resolution:
IP20 is often referred to as the "finger safe" rating for electrical components. It refers to the fact that a probe, the approximate size of a finger, must not be able to access or make contact with hazardous, energized parts. The following short lug covers provide IP20 protection for mechanical lugs and are compatible with control wire terminals (all 1 shield; order 2 for covers for both sides):
H frame, 60 amp: S37446
H frame, 150 amp: S37447
J frame, 250 amp: S37448

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings