Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the wire binding torque requirement for the lugs on a 800A main lug and neutral I-line panel?
Issue:
What is the wire binding torque requirement for the lugs on a 800A main lug and neutral I-line panel?

Product Line:
I-Line circuit breaker panelboards and accessories.

Environment:
Installation

Resolution:
340 in-lbs or 28 ft-lbs

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings