Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can you mount an MA or MH frame breaker in a HCP I-Line type panelboard?
Issue:
Can you mount an MA or MH frame breaker in a HCP type panel?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
I-Line panelboards and circuit breakers sold and supported in the USA.

Cause:
Can the MA/MH circuit breaker be mounted in the HCP I-Line panelboard?

Resolution:
No, The MA breaker mounts differently from other types of breakers, and will not work in an HCP interior. Use the Powerpact M or P frame breaker in the HCP style interior.

The HCR-U interior is the only current design interior that accepts the MA/MH frame breakers.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings