Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a 250A subfeed lug kit type SL250 be installed in a HCN I-Line panels?

Issue:
Installation of higher amperage subfeed lug kit for HCN I-Line panels.

Product Line:
Panelboards

Environment:
I-Line HCN Panelboards

Resolution:
No. The maximum subfeed lug kit that can be installed in an HCN panel is an SL100, which is rated 100A.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings