Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are lugs for circuit breakers rated for compact aluminum conductors?
Issue:
Are Square D breaker lugs rated for use with compact aluminum wire?

Product Line:
Circuit Breakers

Resolution:
Based on UL 486A-486B (paragraph 1.2), compact aluminum conductors (also referred to as "compacted" aluminum) may be used with Square D circuit breaker lugs rated for use with aluminum conductors. The AWG or kcmil rating of the lug must be observed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings