Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the length of the S29343 telescoping shaft for the Powerpact H and J frame breakers?
Issue:
What dimension is needed for mounting the S29343 telescoping shaft?
Product Line:
Circuit Breakers
Resolution:
The distance from the back of the breaker to the front of the panel door is 9.8 inches minimum to 23.5 inches maximum.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings