Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What type of wire binding screw is used with AL150HD lugs and what size it? What is the size or type of tool that is used to torque them?
Issue:
What size Allen wrench should be used on AL150HD?

Product Line:
Powerpact H-Frame

Resolution:
An Allen wire binding screw is used and a 3/16 in Allen wrench is needed to torque screws to 50 in-lbs for #14 - #10 AWG and 120 in-lbs for #8 - 3/0 Al/Cu conductors.

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings