Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the wire range for a NQN6CU 600A 100% neutral kit?
Issue:
Wire range for an NQN6CU 400A and 600A 100% neutral kit

Product Line:
Panelboards and accessories

Environment:
Installation

Cause:
Selectoin

Resolution:
The two lugs in this kit accept 1/0 to 750 kcmil. Al or Cu wire.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings