Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a single pole I-Line circuit breaker available that is rated at 600 Volts?
Issue:
Is a single pole I-Line circuit breaker available that is rated at 600 Volts?

Product Line:
I line panelboards

Resolution:
The single pole, B frame I-Line breakers are rated 347 volts per pole (600Y/347 V system). If there is a requirement for a single pole, 600 V phase-to-neutral breaker, it is advisable to use a two pole (ie. BDA260201) and only use one of the poles.

Schneider Electric USA
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
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalogue
  • Blog
  • Events
  • Schneider Electric Community
  • Sustainability
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings