Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Does the push to test feature on the ground fault modules of the PowerPacT H or J frame require an external 12 VDC to power the shunt trip coil?
Issue:
How does the push to test on GFM modules work?

Product Line:
Molded Case Circuit Breakers

Resolution:
The ground fault module is fault powered to power the 12 VDC shunt trip during an actual fault, but requires a 120 VAC external source wired to terminals 7 and 8 to operate the test feature.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings