Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is it possible to get two accessories, such as a shunt trip and aux contacts, inside of a two pole HD or HG breaker?
Issue:
Is it possible to get two accessories, such as a shunt trip and aux contacts, inside of a two pole HD or HG breaker?

Product line:
PowerPacT H frame

Resolution:
It is possible to install both a shunt trip and a 1A /1B aux contact in the 3 wide, two pole H frame breaker. However, auxiliary contacts are limited to 1A/1B option only because of space limitations.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings