Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do off the shelf panelboard interiors such as HCP32688 & HCP23594 include a sticker that label them as usable for 3 phase, 4 wire applications?
Issue:
Panel labeling

Product Line:
Panelboards

Environment:
I-Line HCP

Cause:
Three phase apps

Resolution:
Merchandised panelboards are not labeled as 3 phase, 4 wire because the neutral assembly is optional and must be purchased separately. Factory Assembled panels have the proper sticker, if ordered as 3 phase, 4 wire. A sticker or label is not available separately.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings