Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the Hvir Comet Infrared Viewing Window part numbers?
Issue:
What are the catalog numbers for the HVIR Comet infrared windows?

Product Line:
HVIR Comet Infrared viewing windows.

Environment:
Selection

Cause:
Specification

Resolution:
IRHVIR75LW2, IRHVIR85U3 & IRHVIR100SW4 are the 2`` 3`` & 4`` short wave versions
IRHVIR75LW2, IRHVIR85U3 & IRHVIR105LW4 are the 2``,3``,4`` long wave versions
Can be purchased by distributors or installed by field services. The selection of short or longwave has to do with the type of camera being used.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings