Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do the NQ Nema 4/4X panelboard enclosures use the LP9618 key ?
Issue:
Key for NQ Nema 4/4X panelboard enclosures

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard boxes sold and supported in the USA.

Cause:
Is the standard panelboard replacement key the same for the Nema 4/4X boxes?

Resolution:
No, 80106-456-01 is the replacement key for Nema 4/4X enclosures.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings