Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the FC I-Line Surge Protection Devices obsolete?

Issue:
Are the FC I-Line Surge Protection Devices obsolete?

Product Line:
IMA Units

Environment:
Maintenance

Cause:
Replacement

Resolution:

Yes, due to the obsolescence of the FC breaker, the I-Line configured Surge Protection Devices are obsolete and have been replaced with I-Line HL Surge Protection Devices.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings