Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can a factory assembled, single phase I-Line panel be converted to 3 phase in the field?
Issue:
Conversion of single phase I-Line panel to 3phase.

Product Line:
I-Line

Environment:
Factory built single phase

Cause:
Conversion

Resolution:
No.  The lug landing and lugs must be torqued to factory specifications and are not available for field installation. The panel label will show as 1 phase and the breakers supplied originally will only have A & C phase connection.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings