How can we help you today?

What are the repair parts for the HU462DS, series F5? (may be shown as F05)

Issue:
Field replaceable parts for HU462DS series F05 / F5

Product Line:
Safety Switch

Resolution:
The repair parts for the HU462DS, series F5 (F05) are as follows. No other parts are available. (NOTE: Descriptions below of "left side" and "right side" mean your left or right as you face the front of the switch)
-Line Base - one each of 4056625250 (left side base), 4056622850 (right side base), and 4056702801 (plastic connecting cam) (NOTE: arc suppressor not included)
-Line Base mounting screw - 4020515101 (3 for each line base)
-Arc Suppressor Assembly - HAS0610F (2 required; includes arc suppressor and mounting screw)
-Lug Assembly - CL0306F (includes 6 lugs)
-Mechanism Assembly - 4056646950 (NOTE: handle coupling, cover interlock defeat coupling, and lockplate gaskets may also need replacing)
-Handle Coupling - 4056699850
-Cover Interlock Defeat Coupling - 4056699750
-Handle Assembly - 4056779850 (also recommend replacing lockplate gaskets)
-Lockplate - 4056681201 (also recommend replacing lockplate gaskets)
-Lockplate Gasket - 4050322803 (2 required)
-Lockplate mounting screw - 2194900001 (2 required)
-Ground Lug - 4025101851 (2 required)
-Ground Lug Mounting Screw - 4020514801

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings