Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do the PowerPacT H and J frame breakers need to be derated if used in drawout or plug-in construction?
Issue:
Derating of drawout or plug-in PowerPacT H/J frame circuit breakers

Product Line:
Molded Case Circuit Breakers

Resolution:
The PowerPacT H and J frame standard rated breakers need no further derating. The 100% rated H and J frame breakers must be derated to 80% in plug-in and drawout configuration.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings