Issue:
Is the S29337, S29338 or S29339 padlockable?
Product Line:
Powerpact Breakers
Resolution:
As shipped, the rotary handle can be padlocked in OFF position only. If padlocking in the ON position is required, the rotary handle needs to be modified in the field per instruction bulletin 48940-249-01.
Is the S29337, S29338 or S29339 padlockable?
Product Line:
Powerpact Breakers
Resolution:
As shipped, the rotary handle can be padlocked in OFF position only. If padlocking in the ON position is required, the rotary handle needs to be modified in the field per instruction bulletin 48940-249-01.
Released for: Schneider Electric USA