Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are keys supplied with the 80116-043-51 replacement locking handle for MH-WP enclosures?
Issue:
Keys supplied with the 80116-043-51 replacement locking handle

Product Line:
MH weatherproof panelboard enclosures sold and used in North America

Environment:
Maintenance/replacement

Cause:
Does the key have to be ordered separately when ordering the replacement handle, 80116-043-51?

Resolution:
No, keys must be ordered separately.  The part number for the key is LP9618, one key per part number.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings