Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is there a limit to how many GFI breakers can be put into an NQ panel ?
Issue:
Is there a limit to how many GFI breakers can be put into an NQ panel ?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
NQ panelboards sold and supported in the USA.

Cause:
Total number of GFI breakers that can be installed in an NQ panelboard.

Resolution:
No, although product selector does have a limit of 28 based on pigtail length, pigtails can be spliced in the factory and the field.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings