Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Do the 72 and 84 circuit NQ panels consist of 1 section or 2?
Issue:
72 and 84 circuit NQ panels consists of 1 section

Product Line:
PTFDS - FD Enclosure Systems

Environment:
NQ panelboards sold and used in North America

Cause:
Do the 72 and 84 circuit NQ panelboards take one or two section enclosures?

Resolution:
They consist of one interior each.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings