Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What does the ``C`` at the end of an MH box number, such as MH50C, indicate?
Issue:
What does the "C" at the end o an MH box number, such as MH50C, indicate?

Product Line:
PTFDS - FD Enclosure Systems

Environment:
Panelboard boxes sold and supported in the USA.

Cause:
Welded base channels on a panelboard box enable it to stand alone, not wall mounted.

Resolution:
The box was built with welded base channels.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings