Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Where are the ground bars placed in standard I-line panels?
Issue:
Ground bars location in standard I-line panels

Product Line:
I-Line Panelboards

Environment:
Products sold and used in North America

Cause:
Product Features

Resolution:
Per the 80043-309-15 I-line Instruction Bulletin, page 27, the ground bar mounting locations are identified by the ground symbol, stamped in the back wall of the box.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings