Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are I-Line panelboards rated for use at 400 Hz?
Issue:
Application

Product Line:
Panelboards

Environment:
Typical Application

Cause:
Product design specification.

Resolution:
Yes. I-Line panelboards are rated for 400 hertz.
The circuit breakers must  be rerated for 400 Hz applications.  See 0100DB0101 for rerating information.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings