How can we help you today?

What is the maximum SD card size that the Multi-Loader can handle?



Resolution:
A 2GB SD card can be used.  However, the card supplied is 4GB, so this is a SDHC memory card. It must be formatted in FAT file system to be recognized with the Multi-Loader.
Indeed, if the card is formatted in FAT32 file system (this is the standard for SDHC memory card), the card will be not recognized with the Multi-Loader.
It is possible to format the SDHC memory card with both Windows 7 and XP operating systems.

Schneider Electric USA

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings