Issue:
Part number for the cover screws of an H or J frame breaker
Product Line:
Molded Case Circuit Breakers
Environment:
Replacement parts for Powerpact H & J frame Circuit breakers
Cause:
At times cover screws are lost when removing the cover from the breaker to install accessories
Resolution:
The replacement screws, sold in single quantities, is part number 20205-000-22.
Released for: Schneider Electric USA