Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
SL800 and HCN I-Line Panelboard

Issue:
Will the SL800 subfeed lug kit fit into an HCN I-Line panelboard?

Product Line:
I-Line Panelboards

Environment:
I-Line Panelboards and accessories sold and supported in North America

Cause:
Customer needs to fit the 800 A subfeed lug kit in an HCN I-Line panelboard.

Resolution:
No, it will not. The SL800 will only fit into an HCM, HCP or HCP-SU panelboard.


UPDATE 2018: Note the HCN I-Line panelboards were obsoleted in December, 2014 and replace by the HCM.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings