Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the ground bar for the HCN style I-Line panelboard?
Issue:
Ground bar part number for the HCN I-Line panelboard

Product Line:
I-Line panelboards and accessories sold and supported in North America

Environment:
Selection/maintenance

Cause:
Determining the proper selection of ground bar for specific style I-Line panelboards.

Resolution:
The ground bar for the HCN style I-Line panelboard is PK27GTA.  The HCN interior only accepts H and F frame low amperage breakers.
The ground bar parts are smaller due to the lower amperage breakers

Note: Effective December, 2014, the HCN style panelboard is obsolete, replaced by the HCM panel

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings