Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the surface finish for the 304 and 316 GRADE Nema 4X, stainless steel trims on I line panelboards?
Issue:
Surface finish for the 304 and 316 GRADE Nema 4X SS trims on i-Line panelboards
Product Line:
I Line panelboard
Environment:
Engineering
Cause:
Clarification
Resolution:
Both 304 and 316 stainless steel trims and doors are Brushed finished, not Gloss

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings