How can we help you today?

What is a Initialization Error (InFE) code on the Altivar 61/71 VFDs?

Resolution:

On the ATV61/ATV71, an Initialization Error (InFE) indicates an internal hardware initialization fault. An internal Schneider Electric support discussion also identifies the related display message“Ini.hard int.” as an internal hardware initialization fault.

For troubleshooting, check the control electronics and connections, particularly the ribbon cable between the control board and power board, and make sure it is properly seated. Low control-board voltage or a damaged control block are also possible causes mentioned in the support discussion

If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

Schneider Electric USA

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings