Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What are the rail and deadfront extension part numbers for the NQ column width panels?
Issue:
Rail and deadfront extension replacement for the NQ column width panels

Product line:
NQ column width panelboards sold and supported in North America

Environment:
Installation

Resolution:
There are no deadfront and rail extensions for the NQ 14 inch column width panels.
A solution is to purchase the appropriate main breaker adapter kit to extend the interior.
However a filler plate will have to be fabricated to cover the opening where the main breaker switch is supposed to be.
Note that this does not apply to 20" panelboard interiors.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings