Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the I-Line, NQ, and NF stainless steel enclosures painted or polished?
Issue:
Are the I-Line, NQ, and NF stainless steel enclosures painted or polished?

Product Line:
Panelboards,  Special Stainless Steel Enclosures

Environment:
NQ, NF and I-Line, HCM, HCP, QMB Type 3R, 4X, 4, 5 and 12; UL Listed

Cause:
Customer does not want paint on stainless steel enclosure.

Resolution:
The Stainless Steel enclosures for the I-Line panelboards are #3 polish.  They are not painted.
This includes the NQ and NF Stainless Steel enclosures too.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings