Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the difference between MH68 and MH68D9L3R3
Issue:
Explain the difference between MH68 and MH68D9L3R3

Product Line:
Panelboard Enclosure/Box

Environment:
Panel board Enclosure/Box

Cause:
Difference

Resolution:
The difference is MH68 is 5.75" deep and MH6D9L3R3 is D9 = 9" deep box, L3 and R3 are 3" side gutters on lh and rh side of box per assistance

Schneider Electric USA

Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings