Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is ILBFMHCPLULC?
Issue:
Description of ILBFMHCPLULC

Product Line:
Panelboards

Environment:
I-line 2017 Service entrance kit

Cause:
2017 UL 67 Service entrance requirements

Resolution:
This is a service entrance main breaker barrier kit so certain I-line panelboards will comply with the new 2017 UL 67 requirement.  Kit is not required if 2017 code has not been locally adopted or for feeder panels.  All factory-assembled panels will ship with the barrier if ULSE is chose in Product Selector.

Please contact your local Distributor or Proficient contractor to obtain the IBLF part numbers and to place your order.

For our Distributors and Proficient contractors:  The IBLF part numbers are found in Product Selectors when selecting RTI panels and are based on the I-line panel selected.  Once the part number is known, it can also be ordered as a separate item using EQM or Q2C.

For more information regarding the code please see the link below for a video as well as documentation.

https://www.se.com/us/en/work/products/explore/service-entrance-barriers/

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings