Our Brands

Impact-Company-Logo-English Black-01-177x54

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Can (4) 3/0 cables on a vertically mounted MG breaker be installed in an 800A I-line panel?
Issue:
Can (4) 3/0 cables on a vertically mounted MG breaker be installed in an 800A I-line panel?

Product line:
I-Line Panelboard sold and supported in the USA>

Environment:
Installation/application

Resolution:
The AL1200P24K lug can be used which can accept (4) 3/0 - 500 kcmil Al or Cu.  The catalog number comes one lug per number.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings