Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a 1600A Wall Mounted Panelboard Available?
Issue:
Can a customer purchase a 1600A wall mounted panelboard?

Product Line:
Circuit breaker panelboards

Environment:
Selection

Cause:
Application

Resolution:
No.  Panelboards max out at 1200A and are wall mounted.  A 1600A or higher selection would have to be built as a QED free standing switchboard.  Customer will have to verify there is sufficient space for a switchboard.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings