How can we help you today?

Is there an option to add dc injection to the enclosed ATS22 soft starters?


Resolution:
The ATS22 and enclosed ATS22 soft starters do not have any kind of option for DC injection.   This technology is not supported with RVSS or reduced voltage soft starters.  If you need a DC injection option you may want to consider using a variable speed drive instead of the soft starter.   If you already have ATS22 and want to do some kind of controlled stop it does have torque controlled stop feature in the drive.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings