How can we help you today?

What is the difference in PK1MB Series 1 and Series 2 accessories?

Issue:
How are series 1 and series 2 PK1MB different from each other?

Product Line:
Load Centers

Environment:
Certain obsolete QO load centers that use the PK1MB accessory

Resolution:
The Series 1 PK1MB consists of metal clips which are screwed into the metal mounting rail of specific QO load centers. The Series 1 PK1MB is no longer available.
The Series 2 PK1MB consists of plastic clips which are screwed into the plastic mounting rail of specific QO load centers. The Series 2 PK1MB is still available as of 2/1/2018.
Series 1 and Series 2 are not interchangeable. See the below picture as reference.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings