Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the actual width of an HCM I line panel Surface mount?
Issue:
Verifying if the actual width of HCM type I-line is 32 inches or 32.25 inches for Surface mounting if we measure enclosure from end to end.

Product Line:
I Line Panelboard

Environment:
Products sold in the United States.

Resolution:
All of our trim fronts are slightly wider than the enclosure. It's designed to slightly overhang on each side. For the HCM NEMA 1 enclosures, the width dimension is 32.00 + 0.020 - 0.000 on the INSIDE.  If we take into account the steel thickness, 0.080 + 0.010 - 0.000, you end up with 32.02 + 0.090 + 0.090 = 32.200" wide by Design. The trim front is designed at 32.240", so only 0.040" overhang, or 0.020" on each side if evenly distributed.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings