How can we help you today?

What is the replacement AC coil for the 8501XO and 8501XMO relays?

Issue:
In need of the AC coil replacement for the 8501 X & XM  series relays.

Product Line:
Industrial Relays

Environment:
NEMA Style AC Relays

Resolution:
Please see list below and check first if the part number is still active as some may already be obsolete.

Voltage60 Hz50 Hz
24 VAC9998X239998X24
110-115 VAC-9998X44
120 VAC9998X44-
208 VAC9998X519998X52
220 VAC9998X529998X53
240 VAC9998X53-
277 VAC9998X55-
380 VAC--
440 VAC-9998X62
480 VAC9998X62-
550 VAC-9998X65
600 VAC9998X65-

Schneider Electric USA

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Help Center
  • Contact Sales
  • Find our Offices
  • Where to Buy
  • Tech Support: 877-342-5173
  • Careers
  • Company Profile
  • Investors
  • Newsroom
  • Report a Misconduct
  • Product Documentation
  • Software and Firmware
  • Product Selector
  • Product Replacement
  • DigestPLUS Online Catalog
  • Industries
  • Partners
  • Schneider Electric Community
  • Events
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings