Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
How do we build a panelboard with a phase failure relay?
Issue:
How does a customer obtain a panelboard with a phase failure relay?

Product Line:
Circuit breaker panelboards and accessories

Environment:
Application

Selection:
Specification

Resolution:
Panelboards are factory assembled only with a TIME MARK 2500 phase failure rely, along with a Schneider ST200 capacitor trip unit, a DC shunt trip on the main breaker and a Bussmann fused
disconnect switch.  A 12" end gutter is also supplied  to accommodate these accessories.  Note this is available only on a NEMA 1 enclosure as an end gutter cannot be furnished for NEMA 3R/12,
NEMA 4/4X enclosures.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings