Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are the Powerpact Circuit Breakers series rated with NQOD panelboard?
Issue:
Can an H-frame breaker be series rated with NQOD Panelboard?

Product Line:
Panelboard

Environment:
NQOD Panelboard

Cause:
N/A

Resolution:
Yes. It is series rated with Powerpact QD,QG,QJ,HD,HG,HJ,HL,JD,JG,JJ and JL Circuit breaker. See attached file for the NQOD series rating table.

Schneider Electric USA

Attachment(s)
NQOD series rating.pdf [103 KB]
Explore more
Range:
Category:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Category:
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings