Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Is a 4 pole I-Line breaker available?
Issue:
Is there a 4 pole I-Line breaker?

Product Line:
Circuit Breaker

Resolution:
No, I-line bussing is only available as the 3 phases with no neutral on the bus, so breakers are only available in 1, 2, and 3 pole.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings