Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
What is the maximum branch circuit breaker that can be installed in an HCM I-Line panel?

Article available in these languages: Spanish

Issue:
What is the maximum branch circuit breaker that can be installed in an HCM I-Line panelboard:

Product Line:
I-Line Panelboards sold and supported in the USA.

Environment:
Application

Cause:
Product selection.

Resolution:
250 amp J frame I-Line breaker is the maximum  that will mount in an HCM panel.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings