Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Will Powerpact J frame breakers fit into an HCN I Line interior at 240 V?
Issue:
Replacement breaker for HCN panel

Product Line:
Circuit Breaker

Resolution:
No, a J frame branch breaker will not fit in an I-Line HCN style panel, no matter what the voltage rating is. A 225 A maximum, 240 VAC rated Q Frame breaker is recommended. A Powerpact J frame branch breaker requires, at minimum, an HCM I-Line interior.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings