Our Brands

Schneider Electric USA Website

Welcome to our website.
		
How can we help you today?
Are Powerpact breakers available with I-line jaws on the OFF end?
Issue:
How do you order a Powerpact breaker with the I-line jaw connectors on the OFF end?

Product Line:
Powerpact H, J, L, M, P, R

Resolution:
To get the I-Line shroud and connections on the OFF end of the breaker, put a K in the third catalog number position. For example, HDK36100.

Schneider Electric USA
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
  • Tech Support: 877-342-5173
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings